DC Block

When the DC Block block in the Probe Setup dialog box diagram is selected, you can choose the model number of the DC blocking capacitor being used.

Descriptions and pictures of the DC blocking capacitors are shown to help with identification.