Sequence Trigger Limitations
Sequence trigger have these limitations:
- The High Bandwidth Edge and Edge Then Edge trigger modes are not available.
- With the Pattern trigger mode, a Range trigger condition can be used for Sequence A or Sequence B, but not both.
- You can only use one long timer (>30 ns). Therefore, trigger modes that use timers greater than 30 ns can only be used for either Sequence A or Sequence B, but not both. Some examples of trigger modes where you might use a long timer include Pulse Width, Glitch, Window, Edge Transition, and Timeout.
- With the Edge trigger mode, the Alternating edge slope selection is not available.