Glitch
The Glitch trigger mode triggers on narrow pulses in a waveform.
-
Source — Select one of the analog input channels.
-
Level — Enter the trigger threshold level in the field or use the increase, 50%, or decrease buttons. Other ways to set the trigger level include dragging the "T" trigger level indicator on the left side of a waveform content window or turning the front panel Trigger Level knob .
-
Slope — Select positive or negative glitches.
-
Time — Defines the maximum pulse width that is considered a glitch.