MATLAB Measurements Variables

When Infiniium starts a user-measurement script, the variables listed in the following table are placed in the MATLAB workspace. This includes any variables that you defined with the <Variable> XML element.

Input Variables

Each input variables, except MeasurementData and SoftwareVersion, listed in the following table has two forms. The one listed is for a single input waveform or the waveform 1 of a dual-waveform input measurement. If a second input waveform exists, its variable has the digit "2" appended. For example, SrcData becomes SrcData2 for the second waveform.

Input Variables
Variables Description Data types
Wave Eye
SrcData The input waveform where the waveform consists of y-data values. Values are in volts for electrical signals and Watts for optical signals. ♦
The input data for an eye diagram is a database where the waveform consists of hits-per-pixel arranged in a two-dimensional array ([column][row]). The column index represents increasing time values starting from the waveform's displayed left side to its right side. The row index represents increasing amplitude values that are in volts for electrical signals and Watts for optical signals. ♦
Source The source of the input waveform.
Example: Source = 'Channel 2'
♦ ♦
SourceBw The bandwidth of the input source.
Example: SourceBw = 150000000000.0
♦ ♦
TotalHits The number of hits in eye database.
Example: TotalHits = 2809395
♦
NumCols The number of columns in eye database. ♦
NumRows The number of rows in eye database. ♦
XOrg The time of the first x-axis value of the input waveform value of SrcData.
Example: XOrg = 8.785e-11
♦ ♦
XInc The spacing of the x-axis input waveform values of SrcData.
Example: XInc = 2.232e-13
♦ ♦
XUnits The X units associated with the input waveform. Refer to Valid Measurement Units.
Example: XUnits = 'Second'
♦ ♦
YOrg The time of the first y-axis value of SrcData.
Example: YOrg = -0.42711
  ♦
YInc The spacing of the y-axis values of SrcData.
Example: YInc = 0.0016430
  ♦
YUnits The Y units associated with the input waveform. Refer to Valid Measurement Units.
Example: YUnits = 'Volt'
♦ ♦
BitRate The current value of the 'Data Rate' control.
Example: BitRate = 9953280000.0
♦ ♦
SymbolRate The current value of the 'Symbol Rate' control.
Example: SymbolRate = 9953280000.0
♦ ♦
SrcClipped Set to True if the source data was clipped high or low; otherwise set to False.
Example: SrcClipped = True
♦  
ClipHigh The maximum value that could be present in the source waveform. If SrcClipped is True, check to see which elements of SrcData are equal to ClipHigh to determine which elements were clipped.
Example: ClipHigh = 0.51057
♦  
ClipLow The minimum value that could be present in the source waveform. If SrcClipped is True, check to see which elements of SrcData are equal to ClipLow to determine which elements were clipped.
Example: ClipLow = -0.510869
♦  
IsAvgComplete Flag tells if waveform averaging is complete. Set to True if complete, otherwise False if not complete.
Example: IsAvgComplete = True
♦  
AvgAcqCount The current value of the 'Number of Averages' control in the Averaging tab of the Acquisition dialog if averaging is enabled, otherwise its value is 1.
Example: AvgAcqCount = 1
♦  
Markers Marker information if markers are on source waveform. If a marker is not on, it is not available. ♦ ♦
Example: x = Markers(1).Position
Markers = [struct('Name','X1','Source','Channel 1','Position',5.9853e-10,'Status','Correct')...
struct('Name','X2','Source','Channel 1','Position',6.4853e-10,'Status','Correct')...
struct('Name','X3','Source','Channel 1','Position',8.0353e-10,'Status','Correct')...
struct('Name','X4','Source','Channel 1','Position',8.5603e-10,'Status','Correct')]
MeasurementData A structure for each defined dependent measurement. Up to four dependent measurements can be defined. ♦ ♦
Example: x = MeasurementData(1).Result
MeasurementData = [struct('Name','Amplitude','Result',0.5032,'Status','Correct','Units','Volt','Source1','Channel 1','Source2','')...
struct('Name','Peak-Peak','Result',0.5096,'Status','Correct','Units','Volt','Source1','Channel 1','Source2','')]
HorizontalChange Set to True if a horizontal change has occurred for an input source. This variable is helpful if accumulation is occurring and it needs to reset when a horizontal change occurs. ♦ ♦
VerticalChange Set to True if a vertical change has occurred for an input source. This variable is helpful if accumulation is occurring and it needs to reset when a vertical change occurs. ♦ ♦
YMiddle The Y middle of the display of the input source. ♦ ♦
YDispRange The Y range of the display of the input source. ♦ ♦
SoftwareVersion The Infiniium software version that is being run. ♦ ♦

Output Variables

This topic lists the variables whose values are returned to Infiniium when your script completes. The Result variable must be set in your script. The remaining variables may be returned, if needed.

Output Variables
Variable Type Description
Variables that must be returned by your script
Result float The measured scalar result.
Optional variables that can be returned by your script
Units string Returns the measurement units of the result. Refer to Valid Measurement Units.
Status string Returns the status of the measurement result. The string can be 'Correct', 'Questionable', or 'Invalid'.
ErrorMsg string Returns an error message for the measurement. The error message is displayed in the oscilloscope message area.