Python Measurement Units
| Full Name | Abbreviation (if available) | Notes |
|---|---|---|
| none | ||
| ampere | A | |
| baud | Bd | |
| Bit Error Ratio | BER | |
| bits | ||
| dBm | ||
| decibel | dB | |
| division | div | |
| inch | in | |
| Farad | F | |
| feet | ft | |
| gain | ||
| Henry | H | |
| Hertz | Hz | |
| hits | ||
| hour | ||
| meter | m | |
| minute | min | |
| Ohm | ||
| percent | % | |
| points | pts | |
| ratio | ' : 1' | Do not include apostrophe (') characters as part of the elements contents. The apostrophes show that a space character is required before and after the colon (:) character. For example, <Units>' : 1'</Units> is not valid and will cause an error. However, <Units> : 1</Units> is valid. It is easier and more reliable simply to use the full name "ratio". |
| reflect | ||
| sample | Sa | |
| second | s | |
| Unit Amplitude | UA | |
| Unit Interval | UI | |
| Unknown | U | |
| Volt | V | |
| Watt | W | |
| waveform | wfm |