DUT Connection and Display of Measurement Result

This section explains how to set the DUT connection and perform measurement using E4982A.

Other topics about Basic operations

DUT connection and measurement

  1. Connect the DUT according to the Operation Manual for the test fixture. The measurement result is displayed as shown the below figure.

How to change measurement point

In the above figure, the measurement result is only displayed for the 1 MHz point among the four measurement points (1 MHz, 10 MHz, 100 MHz and 1 GHz) set according to How to set the measurement point (frequency/averaging factor/oscillator level).

Follow these steps to change the measurement point on which you want to perform measurements and display results.

  1. Click the Root Menu button at the top right corner of the screen to display the softkey menu. The softkey menu appears on the right side of the display.
  2. From the E4982A Root softkey menu, select Active Point.

  3. Select the desired measurement point number, which is in this case is 4.

  4. Alternatively, toggle between Stim Prev and Stim Next hardkeys to select the desired measurement point number.

How to change measurement parameters

Set which of the four measurement parameters should appear on the display by following these steps.

  1. Press the Prmtr key. The measurement parameter selection menu appears in the softkey area on the right side of the display.
  2. Select the measurement parameter which you desire to change, in this case Parameter 1  to display the softkey menu of Parameter 1 on the right side of the display.

  3. Select the desired measurement parameter, in this case Ls.

Measurement and display of all set measurement points (list measurement)

In the above figures, only one of the set measurement points is selected for measurement and display. However, measurement and display can also be executed at all of the set measurement points simultaneously by following the below step.

  1. On the single point measurement display, press the List Meas key once to select the list measurement display.

  1. Press the List Meas key again to view the list measurement display in plotting mode.