Use the following procedure to perform Open calibration using the 7-mm calibration kit using Wizard.
Press Cal Wizard to display the Calibration Wizard.

Spin the knurled nut of the 7-mm connector of the test head installed on the test fixture stand to be protruded to its full extent at the top.
Place the Open standard on the 7-mm test head terminal and turn the Open standard clockwise until it is fully secured using the torque wrench.
Click Open to perform the Open calibration.
For more information on setting the DC resistance (Rdc) limit, please see Setting the Limit for DC Resistance (Rdc).