Other topics about Measurement
The trigger source generates a cue signal that initiates a measurement process. Four types of trigger sources are available:
Press Trigger Mode, then select the desired trigger source.
|
Trigger Sources |
Function |
|
Internal (Internal) |
Uses a consecutive signal generated by the firmware as a trigger source. Triggers are sent immediately following the completion of each measurement. |
|
External (External) |
Uses the external trigger input terminal (BNC) or handler interface as a trigger source. |
|
Manual (Manual) |
A trigger is generated by pressing Trigger. |
|
Bus (Bus) |
A trigger is generated through GPIB/LAN/USB. |
When External is selected as a trigger source, click Input Polarity to select trigger polarity.
|
Softkey Label |
Function |
|
Negative |
Detect external trigger with negative edge. |
|
Positive |
Detect external trigger with positive edge. |
The setting for trigger polarity is NOT valid for the external trigger from the handler interface.
Set the pre-measurement wait time for each measurement point.
Press Trigger Mode > Point Delay.
Enter the point delay time.
Set the external trigger delay time at each point. The trigger delay works when the trigger source is set to external.
Press Trigger Mode > Trigger Delay.
Enter an external trigger delay time.