Other topics about Sorting According to Measurement Results
The BIN Count function counts the frequency by incrementing the BIN count corresponding to the BIN Sorting result by 1 each time the measurement ends. The frequency of each BIN can be viewed on the display when necessary.
If BIN Count is turned ON, the BIN frequency corresponding to the result is increased by 1 each time BIN Sorting is run by the measurement.
BIN Count can be turned ON using the following procedure:
Click on the Bin Count softkey to turn ON/OFF the BIN Count.
|
Softkey Label |
Status of BIN Count |
|
Count [ON] |
ON |
|
Count [OFF] |
OFF |
The BIN Count results is listed at the bottom of the LCD display when Comparator is turned ON. To turn ON the Comparator, refer to Turning ON BIN Sorting and Displaying the Result.

The contents of all BIN counts (for example the value in the counter) can be initialized (resetting) to zero using the following procedure:
Press the Analysis key to display the Analysis softkey menu.
Click on the Clear Bin Count softkey to initialize the contents of all BIN counts to zero.