A warning message is displayed in the instrument message/warning area in the lower left part of the display against a red background. Pushing a front panel key or executing :DISP:CCL command clears the message.
This message simply appears on the display, being not known to a remote environment such as a GPIB.
|
Message |
Description |
|
Variable index out of range |
This occurs when the range of parameter n in var(n, index) function of the user defined parameter exceeds the range of 1 to 10. It should be within 1 to 10. When this warning is displayed, :INIT:CONT ON becomes OFF. |
|
Point index out of range |
This occurs when the range of parameter index in var(n, index) function of the user defined parameter exceeds the range of 1 to 201. It should be within 1 to 201. When this warning is displayed, :INIT:CONT ON becomes OFF. |