:INITiate:CONTinuous {ON|OFF|1|0}
:INITiate:CONTinuous?
This command sets/gets the continuous trigger system. This setting is initialized to OFF when the *RST is issued. For more information on the trigger system, see Trigger system.
|
Parameter |
Value |
|
Description |
Sets/gets continuous trigger system |
|
Data type |
Boolean |
|
Range |
ON or 1: Instructs instrument to continuously activate trigger system OFF or 0: Instructs instrument to NOT continuously activate trigger system |
|
Initial value |
:SYST:PRES=1(ON), *RST=0(OFF) |
|
Preset value |
ON or 1 |
{1|0}<newline><^END>
No equivalent key is available on the front panel.