:CALCulate:COMParator:BEEPer:CONDition {FAIL|PASS}
:CALCulate:COMParator:BEEPer:CONDition?
This command is available when the instrument is configured to beep based on the comparator result (for example, after you have issued the :SYST:BEEP2:STAT command by specifying “ON”). The command lets you specify whether the instrument should beep when the DUT fails to meet the comparator sorting criteria (not sorted into any of bins 1 through 13, or sorted into the NO GOOD bin specified with the :CALC:COMP:OGB command) or when the DUT satisfies the comparator sorting criteria (sorted into the GOOD bin).
|
Parameter |
State |
|
Description |
Instructs the instrument to beep when the DUTs either meet or does not meet the sorting criteria |
|
Range |
Select from the following:
|
|
Preset value |
FAIL |
{FAIL|PASS}<newline><^END>
No equivalent keys are available on the front panel.