:CALCulate:COMParator:COUNt[:STATe] {ON|OFF|1|0}
:CALCulate:COMParator:COUNt[:STATe]?
Lets you specify whether to use the comparator counter. Enabling this feature causes the instrument to count the number of DUTs put into each bin based on the comparator result.
The maximum count value is 2,147,483,647 (231-1). If this value is exceeded, the count value remains 2,147,483,647 and is not updated.
The count value is not reset by execution of reset commands (*RST or :SYST:PRES).
|
Parameter |
State |
|
Description |
ON/OFF the bin counter feature |
|
Range |
Select from the following: ON or 1: Enables the bin counter feature OFF or 0: Disables the bin counter feature |
|
Preset value |
OFF or 0 |
{1|0}<newline><^END>
No equivalent keys are available on the front panel.