:CALCulate:COMParator:DATA:BCOunt?
:CALCulate:COMParator:DATA:BCOUnt? (Syntax for 4287A compatibility)
Returns the count for each bin from the comparator bin counter. The command returns all of the bin counts, regardless of whether the instrument is configured to sort DUTs for each bin. (Query only)
The syntax is changed because BCOU does not meet the SCPI syntax rule. However, BCOU is still accepted for compatibility with the 4287A.
{numeric 1},...,{numeric 14}<newline><^END>
|
Description |
|
|
{numeric 1} |
Count for bin 1 |
|
{numeric 2} |
Count for bin 2 |
|
{numeric 3} |
Count for bin 3 |
|
{numeric 4} |
Count for bin 4 |
|
{numeric 5} |
Count for bin 5 |
|
{numeric 6} |
Count for bin 6 |
|
{numeric 7} |
Count for bin 7 |
|
{numeric 8} |
Count for bin 8 |
|
{numeric 9} |
Count for bin 9 |
|
{numeric 10} |
Count for bin 10 |
|
{numeric 11} |
Count for bin 11 |
|
{numeric 12} |
Count for bin 12 |
|
{numeric 13} |
Count for bin 13 |
|
{numeric 14} |
Count of DUTs that were not sorted into any of bins 1 through 13 (comparator result is 0) or were sorted into NO GOOD bins (set by :CALC:COMP:OGB command). That is the count for a measurement when the /OUT_OF_GOOD_BINS signal of the handler interface changes to LOW level. |
No equivalent keys are available on the front panel.