:CALCulate:COMParator:DATA:BIN?
Returns the most recent comparator result. (Query only)
{0|1|2|3|4|5|6|7|8|9|10|11|12|13|14}<newline><^END>
|
|
Description |
|
0 |
Indicates a DUT that was not sorted into any of bins 1 through 13 |
|
1 |
Indicates a DUT that was sorted into bin 1 |
|
2 |
Indicates a DUT that was sorted into bin 2 |
|
3 |
Indicates a DUT that was sorted into bin 3 |
|
4 |
Indicates a DUT that was sorted into bin 4 |
|
5 |
Indicates a DUT that was sorted into bin 5 |
|
6 |
Indicates a DUT that was sorted into bin 6 |
|
7 |
Indicates a DUT that was sorted into bin 7 |
|
8 |
Indicates a DUT that was sorted into bin 8 |
|
9 |
Indicates a DUT that was sorted into bin 9 |
|
10 |
Indicates a DUT that was sorted into bin 10 |
|
11 |
Indicates a DUT that was sorted into bin 11 |
|
12 |
Indicates a DUT that was sorted into bin 12 |
|
13 |
Indicates a DUT that was sorted into bin 13 |
|
14 |
Indicates sort failed (due to a measurement error) |
If the comparator feature is disabled, the command returns the sorting result from when the comparator feature was last enabled. However, the command returns zero if the E4982A has been reset or the comparator feature has not been enabled since turning ON the E4982A.
No equivalent keys are available on the front panel.