:CALC:COMP:RDC:LIM

Syntax

:CALCulate:COMParator:RDC:LIMit <numeric 1>,<numeric 2>

:CALCulate:COMParator:RDC:LIMit?

Description

Sets the limit range for the Rdc limit evaluation. The limit range is inclusive of both upper and lower limit values.

Variable

 

<numeric 1>

<numeric 2>

Description

Lower limit value*1

Upper limit value*1

Range

-1E20 to 1E20

-1E20 to 1E20

Preset value

0

10000

Unit

Ω (ohm)

Ω (ohm)

Resolution

1E-20

1E-20

  • *1 If <numeric 1> is greater than <numeric 2>, the instrument uses <numeric 1> as the upper limit and <numeric 2> as the lower limit.

If your specified parameter is beyond the valid range, the instrument ignores the parameter and uses either the maximum or minimum value depending on whether the parameter is greater than the upper limit or smaller than the lower limit.

Query response

{numeric 1}, {numeric2}<newline><^END>

The returned data always lists the lower and upper limits in that order.

Related objects

:SOUR:LIST:RDC

Equivalent key

Stim Table > Comparator tab > Bin{1-13} > Rdc Limit  > Upper > <numeric>, or

Analysis > Edit Comptr Table > Bin{1-13} > Rdc Limit  > Lower > <numeric>