*TRG
If the trigger mode is set to GPIB/LAN/USB (BUS, with the :TRIG:SOUR command), this command triggers the E4982A and, after completion of measurement, reads out the measurement data.
This command responds to a query even though it is not suffixed with “?”.
Same as the :FETC? command.
No equivalent key is available on the front panel.