:TRIGger[:SEQuence1]:SOURce {INTernal|MANual|EXTernal|BUS}
:TRIGger[:SEQuence1]:SOURce?
Lets you select one of the following four trigger sources:
Internal
Configures the instrument to use its internal trigger source so that is it automatically and continuously triggered.
Manual
Configures the instrument to be triggered when you press the [Trigger] key on the front panel.
External
Configures the instrument to be triggered when a trigger signal is input through the Ext TRIGGER terminal or handler interface.
GPIB/LAN
Configures the instrument to be triggered when the *TRG is issued.
|
Parameter |
String |
|
Description |
Trigger source |
|
Data type |
String |
|
Range |
INTernal: Internal trigger source MANual: Manual trigger EXTernal: External trigger source BUS: GPIB/LAN trigger |
|
Preset value |
INTernal |
{INT|MAN|EXT|BUS}<newline><^END>
Trigger Mode > Internal|Manual|External|Bus