:SOURce:LIST:POINt <numeric>
:SOURce:LIST:POINt?
Specifies the measurement point for single-point measurement. This setting is retained even if the active table is changed. If the specified point number exceeds the maximum point number allowed in the new active table, however, the instrument will perform single-point measurement using that maximum number instead of the previously specified number.
This setting is reset when settings in the measurement point setup table are changed by execution of the :SOUR:LIST or :SOUR:LIST:CLE command.
|
Parameter |
Value |
|
Description |
Point number for single-point measurement |
|
Data type |
Long integer type (Long) |
|
Range |
1 to 201 |
|
Preset value |
1 |
|
Resolution |
1 |
If your specified parameter is beyond the valid range, the instrument ignores the parameter and uses either the maximum or minimum value depending on whether the parameter is greater than the upper limit or smaller than the lower limit.
{numeric}<newline><^END>
No equivalent key is available on the front panel.