:SOURce:LIST:STATe {ON|OFF|1|0}
:SOURce:LIST:STATe?
This command sets/gets the measurement points to be used during measurement.
List measurement: The instrument measures the DUT’s characteristics at all points defined in the active table. The list mode or plotting mode can be selected by the :DISP:LIST:TYPE command.
Single-point measurement: The instrument measures the DUT’s characteristics only at the point specified by issuing the :SOUR:LIST:POIN command.
|
Parameter |
State |
|
Description |
Sets/gets the measurement points |
|
Data type |
Boolean |
|
Range |
ON or 1: Instructs instrument to perform list measurement OFF or 0: Instructs instrument to perform single-point measurement |
|
Preset value |
OFF or 0 |
{1|0}<newline><^END>
List Meas