:TEST:HANDler:BIN <numeric>
This command can set the output of the Bin No on the handler interface for test purpose and can be used to check/troubleshoot the Test pin signal of Handler interface. To use this command, :TEST:HANDler:MODE should be set to ON.
|
Parameter |
Numeric |
|
Description |
Selection of Handler Interface Test mode on/off |
|
Range |
0: OUT_OF_GOOD_BIN (Handler I/F Pin no. 10) 1 to 13: BIN 1 to 13 (Handler I/F Pin no. 1 to 9 and 19 to 21) 14: All Off |
|
Resolution |
1 |
No equivalent keys are available on the front panel.