:TEST:HANDler:STATus:ALARm {ON|OFF|1|0}
This command sets the output of the alarm pin (pin no. 29) on the handler interface for test purpose. This can be used to check/troubleshoot for the handler interface operation. To use this command, :TEST:HANDler:MODE should be set to ON. As this pin is active-low, output signal level becomes low when it is turned on.
|
Description |
Set the alarm pin status on the handler interface |
|
Range |
ON or 1: Low OFF or 0: High |
No equivalent keys are available on the front panel.