:TEST:HANDler:STATus:KEYLock?
This command gets the status of the key lock pin (pin no. 25) on the handler interface for test purpose. This can be used to check/troubleshoot for the handler interface operation. To use this command, :TEST:HANDler:MODE should be set to ON. As this pin is active-low, 1 is returned when input signal level is low.
|
Description |
Status of the key lock pin on handler interface |
|
Range |
ON or 1: Input Key Lock state is ON. Since the /KEY_LOCK signal is active low, input signal level is low. OFF or 0:Input key Lock state is OFF. Since the /KEY_LOCK signal is active low, input signal level is high. |
|
Preset value |
OFF or 0 |
{1|0}<newline><^END>
No equivalent keys are available on the front panel.