:TEST:HANDler:STATus:TRIGger?
This command gets the status of the trigger pin (pin no. 12 and 13) on the handler interface for test purpose. This can be used to check/troubleshoot for the handler interface operation. To use this command, :TEST:HANDler:MODE should be set to ON.
|
Description |
Status of trigger pin on handler interface |
|
Range |
ON or 1: Input level is high. OFF or 0:Input level is low. |
{1|0}<newline><^END>
No equivalent keys are available on the front panel.