:TRIGger[:SEQuence1][:IMMediate]
When the trigger system is in trigger event detect state, you can use this command to immediately trigger the instrument to start measurement, regardless of the trigger setting. If the trigger system is not in trigger event detect state, however, issuing the command generates an error. For more information on the trigger system, see Trigger system. (No query)
Trigger