Compensation Kit Setup

The compensation kit setup display shown in the following figure appears when you press the Stim Table key the required number of times.

Compensation kit setup tab

When the Compen Kit tab is displayed in front of the other three tabs, the screen shows the compensation kit setup display. If another setup display appears, click this tab with the mouse or press Stim Table key several times to get the compensation kit setup display.

Compensation kit selection

You can choose either to use the predetermined value for the 7-mm calibration kit (7-mm standard) or user-defined value as the compensation kit definition. To use the 7-mm calibration kit, select Default. In case of selecting Default, all compensation kit values should have been entered and you are not allowed to change the definition.

If you select User Defined, you are allowed to enter the values for the compensation kit definition. If you select the Fixed Model, enter the definition for measurement point number 1, which is then automatically applied to the other measurement point numbers.

Table number

Highlights the active table number. The E4982A has eight tables and each table allows a maximum of 201 measurement points to be set. Use the measurement point setup display to set the measurement point conditions (measurement frequency, averaging factor, oscillator level for the measurement point number) for each table.

Measurement point number/measurement frequency

Displays the measurement points (measurement point number and measurement frequency) in the selected measurement point table.

Open standard value

Enter the open standard value.

Short standard value

Enter the short standard value.

DC standard value

Enter the compensation kit definition for E4982A DC resistance (Rdc) measurement.