Other topics about Setting Control Functions
The E4982A is provided with a built-in speaker for emitting beep sounds. The beep sounds serve two functions as shown in the table below.
|
Type |
Function |
|
Completion beep |
Beep sound heard when saving of calibration data or measurement data is completed. |
|
Warning beep |
Beep sound heard when a warning message is displayed or when the result of the BIN sort function (comparator) is "pass" or "fail". |
The warning beep sounds slightly longer than the completion beep.
The following procedure is used to turn the completion beep ON or OFF.
Press System > Misc Setup > Beeper > Beep Done to switch the completion beep ON/OFF.
Clicking Play Beep Done allows you to hear and check the beep tone of the completion beep.
The following procedure is used to turn the warning beep ON or OFF.
Press System > Misc Setup > Beeper > Beep Warning to switch the beep warning ON/OFF.
Clicking Play Beep Warning allows you to hear and check the beep tone of the warning beep.
You can also press the F3 function key (at default setting) to toggle beep warning.
The following procedure is used to set whether the beep sound indicates that the BIN sort function is "Pass" (entered in good BIN) or "Fail" (not entered in good BIN).
Press System > Misc Setup > Beeper > Beep Comparator (or Analysis > Beep Comptr) to switch the beep comparator to Pass/Fail.
To turn the beep comparator OFF, follow the procedure describe in Turning the warning beep ON or OFF.