Other topics about Setting Up the Display of Measurement Results
Traces 1 and 2 each provide two different trace types: data and memory. The data trace keeps track of the DUT's characteristics as it is being tested, while the memory trace captures the measurement data at a specific point in time and displays that data. With the data trace, you can perform a simple calculation on the measurement data and display the results. For example, you can display the differential between the measured data and the memory trace data or the result of subtracting your specified offset value from the measured data. Table below lists the trace types and their functions:
|
Trace Types |
Function |
|
|
Trace 1 |
Data trace (yellow1) |
Displays measurement data/calculations (updated during measurement cycle) |
|
Memory trace (green1) |
Stores and displays previously measured data (captures data when Display > Data -> Memory is selected) |
|
|
Trace 2 |
Data trace (blue1) |
Displays measurement data/calculations (updated during measurement cycle) |
|
Memory trace (brown1) |
Stores and displays previously measured data (captures data when Display > Data -> Memory is selected) |
|
1 Factory default settings.
These features add flexibility to your testing task; for example, on the same screen you can compare the data and memory traces with each other or simultaneously display the results of a calculation as shown by the data and memory traces.
Activate the trace for which you want to perform calculation or comparison between the two trace types.
Press the Display key to display the Display menu.
Press Display > Data.
Start testing the DUT so that the data trace displays the results.
At this time, you may want to hold (stop) the sweep cycle for the data trace by pressing Trigger > Hold. Doing so ensures that you can create an exact snapshot of the measurement data when you later store the data into the memory trace.
Press Data -> Memory to store the measurement data into the memory trace.
When you press Data -> Memory, the memory trace captures the measurement data exactly as it is displayed on screen. The memory trace always stores measurement data, even when the data trace is displaying the results of a calculation. Note that while the subtraction of the offset value is being executed, the resulting subtraction is stored in the memory trace. The Data -> Memory key affects both Traces 1 and 2. This means that the measurement data for the non-active trace is also stored into the memory trace.
The Keysight E4990A provides a number of options that allow you to control how each trace is displayed. Select one of the following display options by pressing the appropriate key:
|
Softkey |
Function |
|
Data |
Displays only data trace on the screen |
|
Mem |
Displays only memory trace stored by Data -> Mem operation on the screen |
|
Data & Mem |
Displays data trace and memory trace on the screen. You can now easily compare the data trace and memory trace on the screen. |
|
Off |
Trace is not displayed |
Start testing the DUT to obtain the measurement data for comparison or calculation with the reference measurement data you stored into the memory trace (if the sweep cycle is in the hold state, you can restart the measurement by pressing Trigger).
You can specify an offset value to be subtracted from the measurement data, and the result of this operation is displayed by the data trace.
Press Display > Data -> Mem to store the measured data in memory.
Press Data Math Offset and input the desired offset value (the offset value defaults to zero in the preset state).
Press Data Math.
Select the data math operation to perform.
|
Softkey |
Function |
|
OFF |
Turns off data math functions (Do not perform data math) |
|
Data / Mem |
Divides measured data by memory trace and stores result in data trace |
|
Data * Mem |
Multiplies data trace by memory trace and stores result in data trace |
|
Data - Mem |
Subtracts memory trace from data trace and stores result in data trace |
|
Data + Mem |
Adds data trace and memory trace and stores result in data trace |
Press Display.
Select the type of data on display ON the screen.
Send the trigger to make measurements.