Other topics about Maintenance
This section describes how to clean the instrument.
To protect yourself from electrical shock, be sure to unplug the power cable from the outlet before cleaning the instrument.
Never clean the internal components of the instrument.
Use one of the following methods to clean the display surface regularly.
For normal cleaning, rub the surface gently with a dry, soft cloth.
When stains are difficult to remove, gently wipe the surface with cloth damped with a small amount of dehydrated ethanol.
You can clean the standard LCD (no touch screen function) with a cloth dipped in water and then wrung tightly.
Do not use chemicals other than dehydrated ethanol to wet the cleaning cloth. To clean the touch screen LCD, do not wet the cloth with water.
The ports of the E4990A are fitted with BNC connectors. Stains or other damage to these connectors would significantly affect the accuracy in measurements. Always pay attention to the following precautions.
Always keep the connectors free from stains and dust.
Do not touch the contact surface on the connectors.
Do not plug damaged or scratched connectors into the test ports.
Use compressed air for cleaning connectors. Do not use abrasives under any circumstance.
The above precautions must also be observed in maintaining connectors and ports other than these test ports.
To remove stains on parts other than the LCD, test ports, and other connectors/ports of the instrument, wipe them gently with a soft cloth that is dry or wetted with a small amount of water and wrung tightly.