Command/Query
:CALCulate<Ch>[:SELected]:DATA:FDATa <Value>
:CALCulate<Ch>[:SELected]:DATA:FDATa?
This command sets/gets the formatted data array.
The array data element varies in the data format. If valid data is not calculated because of the invalid measurement, “1.#QNB” is read out.
|
Parameter |
Value |
|
Description |
Formatted data array Where n is an integer between 1 and NOP (number of measurement points):
The number of data is {NOP×2} |
|
Data Type |
Variant type Array (Range) |
|
Note |
If there is no array data of NOP×2 when setting a formatted data array, an error occurs when executed. |
{numeric 1}, .... ,{numeric NOP×2}<newline><^END>
See Reading/Writing Data.
No equivalent key is available on the front panel.
SCPI.CALCULATE(Ch).SELECTED.DATA.FDATA