Command
*RST
This command presets the E4990A to its default settings and is different from setting state preset with the :SYST:PRES as the continuous initiation mode (see :INIT:CONT) of channel 1 is set to OFF.
Ana.WriteString "*RST", True
No equivalent key is available on the front panel.
SCPI.IEEE4882.RST