:SYST:UPR

Type

Command

Syntax

:SYSTem:UPReset

Description

This command presets the E4990A with the user settings. The command is executed regardless of the operation mode in preset state.

If you try to specify a file for a preset (D:\UserPreset.sta) that does not exist, a warning message will be displayed and  :SYST:PRES will be executed.

Examples

Ana.WriteString ":SYST:UPR", True

Related Commands

*RST

:SYST:PRES

Equivalent Softkey

Preset (When System > Misc Setup > Preset Setup > State > User is selected.)

COM Command Syntax (Internal Control Only)

SCPI.SYSTEM.UPRESET