To use the DUT connecting terminal as a calibration plane, you only need to execute calibration for open/short/load.

Measure the calibration data according to the following procedure:
The definition of the calibration kit used should be changed as needed. For more on this procedure, see Defining Standard Values for User Calibration.
Connect a test fixture in front of the 7-mm terminal. For more on the connecting method, see the fixture’s operation manual.
Measure the calibration data of open/short/load at the DUT connection terminal (used as a calibration reference plane). For more on this procedure, see Calibration of Open/Short/Load/Low-loss Capacitor. (Note that low-loss capacitor calibration is not performed.)
Other topics about Calibration