The electrical lengths of the test fixtures shown below have been registered in the E4991B in advance. To use these fixtures, you may set the needed electrical length by simply selecting the model number of the fixture to be used. If you use fixtures that are not registered, however, you must enter the electrical length as a numerical value.
|
Model Number |
Electrical Length |
|
16191A |
14 mm |
|
16192A |
11 mm |
|
16193A |
14 mm |
|
16194A |
50 mm |
|
16196A |
26.2 mm |
|
16196B |
26.9 mm |
|
16196C |
27.1 mm |
|
16196D |
27.3 mm |
|
16197A |
14 mm |
|
16198A |
N/A |
|
16453A |
0 mm |
|
16454A (Fixture size: S) |
0 mm |
|
16454A (Fixture size: L) |
0 mm |
Press Cal > Accessory > select the fixture model number. To select a test fixture that is not registered, select Arbitrary.
If Arbitrary is selected, press Cal > Accessory Length > enter the fixture length.
Other topics about Calibration