Other topics about Setting Measurement Conditions
Follow the steps below to specify a fixed frequency for the signal source when the sweep parameter is any item other than frequency (i.e., oscillator level or DC bias).
Press Sweep Setup.
Press CW Freq and input the desired fixed frequency value.
Press Sweep Setup > OSC Level to display the oscillator level settings menu.
Press OSC Unit and select your desired oscillator level from the Voltage | Current | Power option.
Press Sweep Setup > OSC Level to display the oscillator level settings menu.
The Voltage Level , Current Level or Power Level is enabled depending on your oscillator selection. For example, if you have selected OSC Unit > Voltage, then Voltage Level is enabled. then, press the Voltage Level and input the desired voltage level value.
Follow the steps below to apply DC bias to DUT, regardless of whether you plan to sweep by DC bias.
Press Sweep Setup > DC Bias > DC Bias Mode to display the DC bias mode selection options.
Select one of the DC bias mode, either Voltage or Current.
When the sweep parameter is not DC bias, select the DC bias mode and then follow the steps below to set DC bias level.
Press Sweep Setup > DC Bias to display the DC bias selection options.
The Voltage Level or Current Level is enabled depending on your DC bias mode selection. For example, if you have selected DC Bias > DC Bias Mode > Voltage, then Voltage Level is enabled. then, press the Voltage Level and input the desired voltage level value.
Follow the steps below to set limit values for the voltage or current in order to protect the DUT being measured.
Press Sweep Setup.
Press DC Bias > Limit Voltage | Limit Current and input the limit value.
Press Sweep Setup.
Press DC Bias > DC Bias State and toggle between the ON|OFF selection to turn ON/OFF the DC bias state.
Turning DC bias ON displays DC ON at the instrument bar in the lower right area of the screen.
DC bias source can be turned off during hold state. This status is kept after the preset.
Press System.
Press Service Menu > DC Output @Hold and toggle between ON and OFF.