Setting for Phase

Other topics about Setting Up the Display of Measurement Results

Selecting the Phase Unit

When you are performing phase-based measurement, you can specify whether to use degrees or radian as the phase unit applied to the scaling and marker features.

  1. Activate the trace for which you want to set the phase unit.

  1. Press the Format key to display the Format menu.

  2. Press Phase Unit > Deg|Rad to select your desired phase unit.

Displaying Phase Values without Wrapping at ±180 degree

The E4991B provides a feature that allows you to display phase values without wrapping them at +180° or -180°. This feature, called “expanded phase,” is useful when measured phase values are in a continuous increase or decrease and some of them exceed +180° or -180°. To set up the expanded phase feature, follow these steps:

  1. Activate the trace for which you want to use the expanded phase feature.

  1. Press the Format key to display the Format menu.

  2. Press Expand Phase > ON|OFF to turn On or Off the expanded phase feature.