:CALC<Ch>:EPAR:SIM

Type

Command

Syntax

:CALCulate<Ch>:EPARameters:SIMulate[:IMMediate]

Description

This command writes the simulation results into the memory trace, then set "Data & Mem" for the display setting. All traces related with impedance measurement are updated, even if :CALC:EPAR:SIM:AUTO is set at OFF.

Examples

Ana.WriteString ":CALC1:EPAR:SIM", True

Related Commands

:CALC:EPAR

:CALC:EPAR:DISP

:CALC:EPAR:SIM:AUTO

Equivalent Softkey

There is no equivalent key is available on the front panel. However, the similar key is:

Analysis > Equivalent Circuit > Simulate

COM Command Syntax (Internal Control Only)

SCPI.CALCULATE(Ch).EPARAMETERS.SIMULATE.IMMEDIATE