Command/Query
:CALCulate<Ch>:MATerial:DIELectric:THICkness <Value>
:CALCulate<Ch>:MATerial:DIELectric:THICkness?
This command sets/gets the thickness of material for dielectric measurement.
|
Parameter |
Value |
|
Description |
The thickness of the material for dielectric measurement |
|
Data Type |
Numeric type (Real) |
|
Range |
1u ~ 4.8m |
|
Preset Value |
1u |
|
Unit |
m |
|
Resolution |
- |
{numeric}<newline><^END>
Dim Var as Double
Var= 0.000001
Ana.WriteString ":CALC1:MAT:DIEL:THIC " & Str(Var), True
Ana.WriteString ":CALC1:MAT:DIEL:THIC?", True
Var=Ana.ReadNumber
Measurement > Material Dimension > Thickness
SCPI.CALCULATE(Ch).MATERIAL.DIELECTRIC.THICKNESS