Command/Query
:FORMat:DATA {ASCii|REAL|REAL32}
:FORMat:DATA?
This command can be used to set/get the format data using the following SCPI commands:
|
Parameter |
Selection Option |
|
Description |
Data transfer mode |
|
Data Type |
Character string type (String) |
|
Range |
ASCii: ASCII transfer format REAL: IEEE 64-bit floating point binary transfer format REAL32: IEEE 32-bit floating point binary transfer format |
|
Preset Value |
ASCii |
{ASC|REAL|REAL32}<newline><^END>
Dim Var as String
Var= "ASC"
Ana.WriteString ":FORM:DATA " & Var, True
Ana.WriteString ":FORM:DATA?", True
Var=Ana.ReadString
No equivalent key is available on the front panel.
SCPI.FORMAT.DATA