*TRG

Type

Command

Syntax

*TRG

Description

This command triggers the E4991B if the trigger source is set to Bus.

Examples

Ana.WriteString "*TRG", True

Related Commands

:TRIG:SOUR

:TRIG:SING

:TRIG

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.IEEE4882.TRG