Command
:TRIGger[:SEQuence][:IMMediate]
This command generates a trigger immediately and executes a measurement, regardless of the setting of the trigger mode.
This command is different from :TRIG:SING as the execution of the object finishes at the time of a trigger.
If you execute this object when the trigger system is not in the trigger wait state (trigger event detection state), an error occurs when executed and the object is ignored.
Ana.WriteString ":TRIG", True
Trigger > Trigger (This is for manual trigger.)
SCPI.TRIGGER.SEQUENCE.IMMEDIATE