Command
:MMEMory:LOAD:SEGMent <Value>
This command load the specified segment table file of active channel from CSV file (file with a .csv extension saved with the:MMEM:STOR:SEGM).
Specify the file name with the extension. When you use directory names and file name, separate them with "\" (back slash), or "/" (slash).
|
Parameter |
Value |
|
Description |
File name (extension ".csv") |
|
Data Type |
Character string type (String) |
|
Range |
254 chars |
Dim Var as String
Var = "D:\segtable1.csv"
Ana.WriteString ":MMEM:LOAD:SEGM " & Var, True
Sweep Setup > Edit Segment Table > Import from CSV File...
SCPI.MMEMORY.LOAD.SEGMENT