:SOUR<Ch>:BIAS:CURR:CENT

Type

Command/Query

Syntax

:SOURce<Ch>:BIAS:CURRent:CENTer <Value>

:SOURce<Ch>:BIAS:CURRent:CENTer?

Description

This command sets/gets the center of bias current value in DC bias sweep.

Variable

Parameter

Value

Description

Center value

Data Type

Numeric type (Real)

Range

-100m ~ 100m

Preset Value

0

Unit

A

Resolution

1μ

Query Response

{numeric}<newline><^END>

Examples

Dim Var as Double
Var= 0.3
Ana.WriteString ":SOUR1:BIAS:CURR:CENT " & Str(Var), True
Ana.WriteString ":SOUR1:BIAS:CURR:CENT?", True
Var=Ana.ReadNumber

Related Commands

:SOUR:BIAS:CURR:SPAN

:SOUR:BIAS:MODE

Equivalent Softkey

Center (in DC Bias current sweep)

COM Command Syntax (Internal Control Only)

SCPI.SOURCE(Ch).BIAS.CURRENT.CENTER