:SOUR<Ch>:BIAS:CURR:SPAN

Type

Command/Query

Syntax

:SOURce<Ch>:BIAS:CURRent:SPAN <Value>

:SOURce<Ch>:BIAS:CURRent:SPAN?

Description

This command sets/gets the span of bias current value in DC bias sweep.

Variable

Parameter

Value

Description

Span value

Data Type

Numeric type (Real)

Range

0 ~ 200m

Preset Value

0

Unit

A

Resolution

2μ

Query Response

{numeric}<newline><^END>

Examples

Dim Var as Double
Var= 0.1
Ana.WriteString ":SOUR1:BIAS:CURR:SPAN " & Str(Var), True
Ana.WriteString ":SOUR1:BIAS:CURR:SPAN?", True
Var=Ana.ReadNumber

Related Commands

:SOUR:BIAS:CURR:CENT

:SOUR:BIAS:MODE

Equivalent Softkey

Span (in DC Bias current sweep)

COM Command Syntax (Internal Control Only)

SCPI.SOURCE(Ch).BIAS.CURRENT.SPAN