:SOUR<Ch>:BIAS:CURR:STAR

Type

Command/Query

Syntax

:SOURce<Ch>:BIAS:CURRent:STARt <Value>

:SOURce<Ch>:BIAS:CURRent:STARt?

Description

This command sets/gets the start of bias current value in DC bias sweep.

Variable

Parameter

Value

Description

start value

Data Type

Numeric type (Real)

Range

-100m ~ 100m

Preset Value

0

Unit

A

Resolution

2μ

Query Response

{numeric}<newline><^END>

Examples

Dim Var as Double
Var= -0.1
Ana.WriteString ":SOUR1:BIAS:CURR:STAR " & Str(Var), True
Ana.WriteString ":SOUR1:BIAS:CURR:STAR?", True
Var=Ana.ReadNumber

Related Commands

:SOUR:BIAS:CURR:STOP

:SOUR:BIAS:CURR:STAR

Equivalent Softkey

Start (in DC Bias current sweep)

COM Command Syntax (Internal Control Only)

SCPI.SOURCE(Ch).BIAS.CURRENT.START