Command/Query
:SOURce<Ch>:POWer:STARt <Value>
:SOURce<Ch>:POWer:STARt?
This command sets/gets the start power
|
Parameter |
Value |
|
Description |
Start power |
|
Data Type |
Numeric type (Real) |
|
Range |
80μ ~ 10.02m |
|
Preset Value |
80μ |
|
Unit |
dBm |
|
Resolution |
100m |
{numeric}<newline><^END>
Dim Var as Double
Var= 0
Ana.WriteString ":SOUR1:POW:STAR " & Str(Var), True
Ana.WriteString ":SOUR1:POW:STAR?", True
Var=Ana.ReadNumber
No equivalent key is available on the front panel.
SCPI.SOURCE(Ch).POWER.START