:SYST:PRES

Type

Command

Syntax

:SYSTem:PRESet

Description

This command presets the setting state of the E4991B to the original factory setting (Default Conditions). This command is different from *RST as the continuous startup mode (:INIT:CONT) of channel 1 is set to ON.

Examples

Ana.WriteString ":SYST:PRES", True

Related Commands

*RST

:SYST:UPR

Equivalent Softkey

Preset (When System > Misc Setup > Preset Setup > State > Factory is selected.)

COM Command Syntax (Internal Control Only)

SCPI.SYSTEM.PRESET