Show 

Connecting External Accessories

The E4991B can be connected to external input/output devices such as printer, monitor, keyboard and mouse.

Other topics about Using Windows

Connecting a Printer

A printer can be connected to the E4991B through any USB ports on the front or rear panels. Its driver may be required to install.

Connecting a Mouse/Keyboard

A USB mouse and USB keyboard can be connected to the E4991B through any USB ports on the front or rear panels.

Connecting a Monitor

A monitor can be connected to the E4991B using the External Monitor Output Terminal (Video) located in the rear panel of the E4991B.