Other topics about Data Output
You can manage the files and folders by using Windows® Explorer, which provides such standard operations as copy, move, remove, change name, and format floppy disk.
Do not change any content (i.e. folders or files) of the drives other than A and F: This may cause serious damage to the E5052B ’s functions and performance.
Press Save/Recall.
Press Explorer... to open Windows Explorer.
In Windows Explorer, select any source file or folder for copying.
On the menu bar, select Edit > Copy.
Open the target folder for copying.
On the menu bar, select Edit > Paste.
In Windows Explorer, select the file or folder of origin.
On the menu bar, select Edit > Cut.
Open the destination folder.
On the menu bar, select Edit > Paste.
In Windows Explorer, select the file or folder to be removed.
On the menu bar, select File > Delete.
In Windows Explorer, select the file or folder for which you want to change name.
On the menu bar, select File > Rename.
Type the new name for the file or folder and then press Enter on the keyboard.