You can save the E5052B’s screen image on a file in the bitmap or PNG format. The saved file can be recalled for later use with PC application software.
Follow the steps below to save the screen image on a file.
Display the screen that you want to save on a file.
Press System to display the system menu. Use the following softkey from the System menu.
|
Softkey |
Function |
|
Dump Screen Image |
Saves the screen information on a file |
The image displayed on the screen just before pressing System is saved in the file.
For more information, refer to Images You Can Print/Save.
Press Dump Screen Image to open the “Save As” dialog box. For information on the Save As dialog box, refer to the description for Save As dialog box. In this case, either Bitmap Files (with the extension of *.bmp) or Portable Network Graphics (with the extension of *.png) is selected as the file type.
Select the file type.
Specify the folder in which you want to save the file and enter the file name. Press Save to save the screen image of the E5052B in a file.